4/5/2016 1:25 PM | |
Joined: 6/3/2014 Last visit: 9/12/2025 Posts: 660 Rating:
|
Hello Stef_VanLoon, synchronization between two or more panels is possible. You can export the recipe of one panel to a shared folder on a PC/drive. Then the other panel can read this recipe. You might need to correct the tag names via script. You could use shared tags in the plc to "remote control" the second panel. USB won't work, because you can't share folders on a USB device connected to a panel. Alternatively you might want to have a look at area pointers: https://support.industry.siemens.com/cs/ww/en/view/109091876/69243865483 https://support.industry.siemens.com/cs/ww/en/view/109091876/23118609803 |
Last edited by: H.J. at: 4/5/2016 1:28:48 PMLast edited by: H.J. at: 4/5/2016 1:31:10 PM~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
This contribution was helpful to
1 thankful Users |
4/14/2016 12:09 PM | |
Posts: 22 Rating:
|
Option1: The best way is to have a network share drive and then both HMIs are pointing to the same excel sheet. Option 2: If the both HMIs have same screens and control functions then. You can use Sm@rt Server and Sm@rt Client function to clone the HMI. HMI1 will become master server. HMI2 will become client. now from HMI2 creates a remote desktop session on the HMI1. So now you can control both HMI and share same data. Hope it helps Thanks |
4/23/2016 7:24 PM | |
Joined: 4/24/2006 Last visit: 9/15/2025 Posts: 9027 Rating:
|
Hello Stef_VanLoon, Please have a look at the following link: How do you integrate an HMI operator panel into a local network? Best regards, Wizard |
Follow us on