12/22/2021 5:55 AM | |
Joined: 12/14/2021 Last visit: 1/7/2025 Posts: 3 Rating:
|
Hello Everyone, I am unable to download the Simatic PC Station to the PLC. it is showing a message "The connection to the target module cannot be established". After adding the WinCC application and IE General to the Rack I have created the S7 connection between IE general and SIMATIC 400(1)/CPU 410 SMART in NetPro. I have set the PG/PC in TCPIP.Auto.1 and put the same IP address, subnet and MAC address to the Ethernet interface of IE general as my desktop and save_and _compiled with no error message. now in the SIMATIC PC Station Hardware configuration window when I try to download to the PLC it shows message "The connection to the target module cannot be established". Please guide me as I am trying to learn and using the SIMATIC Manager first time. Thank you ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/22/2021 12:39:01New subject after splitting |
|
This contribution was helpful to
1 thankful Users |
Follow us on