11/19/2024 9:04 AM | |
Joined: 11/13/2024 Last visit: 2/24/2025 Posts: 1 Rating:
|
Hi guys I hope you'll be fine and doing well. It's been a while that I'm using TIA portal V17, but I have a problem with HMI compiling and simulation. When I define all the tags for HMI correctly and want to simulate it, it says compilation failed and contact siemens support, while I rebuild software many times, but it didn't work. And also, when I want to simulate the HMI project, the WinCC unified runtime should be open automatically like PLSIM, but it doesn't why? I really need to solve those problems, help me those who know. Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 11/19/2024 09:25:52New subject after splitting |
|
11/19/2024 9:59 AM | |
Joined: 5/6/2022 Last visit: 9/15/2025 Posts: 589 Rating:
|
Hi abdullah_harris1, In this case I think we need more information to be able to dig into the situation: - What version of Windows operating system do you have installed? - Screenshot of the Siemens software installed on the PC. To do this, take a screenshot from TIA Portal -> Help -> Installed Software. Do you have any V17 updates? Do you work with Unified? - Screenshot of the exact error you get. - If you create a very simple new project, do you get the same compilation problem? I recommend you also delete the IM folder of the project: "How do I delete the IM folder of my TIA Portal project?" Best regards!
|
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on