10/25/2024 6:59 AM | |
Joined: 2/13/2024 Last visit: 3/14/2025 Posts: 2 Rating:
|
Hola, actualmente estoy usando para programar TIA Portal V19. Tengo un confort panel 900 con una version de 17.0006, en mi proyecto tia portal solo puedo aniadir una tp900 con version V17.0. Estoy leyendo, mirando videos, descargando todo tipo de updates y no tengo resultado. Por favor, me podeis decir paso a paso lo que tengo que realizar y los enlaces donde puedo encontrar lo que tengo que instalar? Un saludo ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 10/25/2024 07:51:03New subject after splitting |
|
10/25/2024 8:16 AM | |
Joined: 1/21/2013 Last visit: 9/15/2025 Posts: 4110 Rating:
|
Hi, The latest device version for a WinCC Comfort panel is V17.0.0.0. However, the device version and the image version do not always match, as the device version is only increased when new features are added or other major changes are made. This usually does not happen within a major release cycle. (At least as for WinCC Basic/Comfort/Advanced). The latest device version (today it is V17.0.0.8) can be downloaded at "Image Downloads for SIMATIC HMI Operator Panels: Comfort / Mobile / Basic Panels". Kind regards |
This contribution was helpful to
1 thankful Users |
Follow us on