8/21/2017 4:09 PM | |
Joined: 9/27/2006 Last visit: 9/2/2025 Posts: 12397 Rating:
|
Hello Hoss; There is a Modbus RTU driver integrated in WinCC v14 that you could probably use. Modbus communications are generally independant of the manufacturer of the device. The manuaI have is for WinCC v14 SP1, if you have a different version look it up in the online help. SIMATIC WinCC WinCC Professional V14 SP1 - CommunicationCommunication with other PLCs (Basic Panels) IntroductionCommunication with other PLCs is communication with PLCs that are not in the SIMATIC family. These PLCs have proprietary protocols for data exchange. The protocols are configured as communication drivers in WinCC. Communication driversThe following communication drivers are supported in WinCC and are already installed:
-Omron Host Link Hope this helps, Daniel Chartier |
Follow us on