10/27/2022 7:36 AM | |
Joined: 9/16/2021 Last visit: 2/8/2024 Posts: 30 Rating:
|
Hi Francisco, I also had kind of similar problem. I wanted to give specific layer rights to specific layer to certain users but giving only layer rights did not work. So, I did something different. If you know you can also manipulate rights for the objects in COMOS not just only for layers.(In the forum it is not possible to attach screenshots yet and it makes it a little difficult to explain). In my attachment look at figure 1. I have given the project in the rights but no specific rights and then I have given layer all the rights, but this is not enough. I also need to give rights for the objects they can edit. The users will not be able to create a new object under layer(by right mouse click), but they will be able to create and change anything for the object that you have given rights for. In this case I'd recommend select the topmost hierarchy after the layer and assign all the rights and it will be enough. In the figure 2 I have illustrated that with drag & drop you can change the object in rights window, and you can then assign rights normally. I hope I understood your requirement right and hope this helps, Regards, Vishal Ramani AttachmentLayers.zip (521 Downloads) |
Follow us on