4/7/2008 4:52 PM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating:
|
Hi, i think somethink must be wrong with the integrated function from WinCC flexible into STEP 7. It is the first time that you work with Alarm S? Did you have this problem only with this project or did you have this problem with "older" projects too? Did you have made a update -> flexible 2005 to 2007? In which order did you have install Step7 and WInCC flexible --> 1. STEP 7 --> 2. WinCC flexible --> OK Are the Version from STEP 7 and WInCC flexible compatible? -> http://support.automation.siemens.com/WW/view/en/22635649 But think you should contact the siemens hotline. regards, |
4/18/2008 10:29 AM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating:
|
Hi, the blue text isa warning only. Does the Runtime works without errors? Bye |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
Follow us on