7/9/2013 11:47 AM | |
Joined: 1/20/2008 Last visit: 7/9/2024 Posts: 120 Rating: (7) |
I'm agree with Ste39. RAM memory is the best solution for commissioning time. After commissioning, it is best to use the Flash EPROM. |
This contribution was helpful to1 thankful Users |
7/10/2013 10:36 AM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating: (705) |
Hi DS SURESH KUMAR, Yes, but then you have to save in EEPROM. S7 400 EPROM |
Last edited by: Ste39 at: 7/10/2013 10:38 AM |
|
7/13/2013 10:05 AM | |
Joined: 11/8/2011 Last visit: 7/2/2024 Posts: 387 Rating: (43) |
Hi Hav a look on this thread Funtion of EPROM |
Follow us on