3/15/2011 8:01 PM | |
Joined: 8/31/2010 Last visit: 6/12/2024 Posts: 1516 Rating: (223) |
I installed in this order 1. WinCC v7.0+SP2 with no updates 2. WinCC v7.0+SP2 + Update 2 3. WinCC v7.0+SP2 + Update 2 When i installed update 2, i had the same problem. Surprisingly the problem was solved on the next day with no reason left for me to guess. Now when i am installing update 3 also i'm having the same issue. Today this error is no more in my PC, i don't know what's happening. Do you have more info on the SIMATIC Rights ? (will be helpful) You mean to say the current user shouldn't be in the Simatic HMI Group, am i rite? To add with I'm having a problem which is not allowing me to activate the Graphics Runtime alone. Refer this pdlrt.exe error. |
Like it? Rate it! |
|
3/16/2011 7:51 AM | |
Posts: 799 Rating: (43)
|
Hi, you will find all the infos about Simatic Rights and the needed user gruoups in this manual. I think this is everything you need to know! best regards |
3/16/2011 11:51 AM | |
Posts: 799 Rating: (43)
|
Have you already contacted technical support? In your second thread, i saw the screenshots, and this is a classical crash of the pdlrt.exe So you have to download the user dump tool from microsoft here. After that you have to configure the tool for an automatic dump of the pdlrt.exe process (Access Violation) (You will find also a description, how to use here) Normally, when you configured right, the dumpfile is created, while next crash of the pdlrt.exe. Contact technical support, they will tell you how to send the files (dumpfile, logfiles, etc). Siemens development will analyse the files and after that they can tell you what the reason is. regards |
3/17/2011 3:49 AM | |
Joined: 8/31/2010 Last visit: 6/12/2024 Posts: 1516 Rating: (223) |
Thanks efka. Will try it out and let you know. |
Like it? Rate it! |
|
7/14/2016 1:34 PM | |
Joined: 11/6/2015 Last visit: 3/4/2024 Posts: 6 Rating: (0) |
@AutoGen_280204Thank you for your Information it helped me a lot |
Follow us on