1/31/2016 4:57 PM | |
Joined: 12/7/2011 Last visit: 9/3/2025 Posts: 386 Rating:
|
Hi to all. I'm here because still now i'm facing with the tren archive problem, posted here Error in Trend Archive. After a lot of test i'm pretty sure that the problem don't coming from the configuration, because also with only one varible stored the problem coming out again. Now i'm moved my attention in a Windows CE, in some forum a read that the Windows CE 5.0 (like the one installed on my MP377) supports up to external 32GB usb, in other i read that is not suggested. Tomorrow i'll do this other test to reduce the capacity of the external key to 8 GB. Does anyone know for certain limitations of Win CE 5.0? Regards. Duccio |
Follow us on