2/14/2011 9:51 AM | |
Posts: 12 Rating:
|
Dear All, So many views and no replies...where are all the experts gone? |
2/15/2011 12:30 PM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello, Are you using a HMI panel or WinCC flexible RT? Have you seen these manuals: SIMATIC HMI WinCC flexible 2008 Communication Part 1 SIMATIC HMI WinCC flexible 2008 Communication Part 2 Best regards, Wizard |
2/16/2011 5:36 AM | |
Joined: 7/28/2010 Last visit: 8/31/2024 Posts: 184 Rating:
|
Hi Ali Asghar, Take a look at the attached page to see what kind of controllers can be connected to a Wincc Flexible Runtime. You can't hook up anything as the wincc flex needs to know the protocol for communicating to the third party unit. Regards, Behnam www.sigmaprocess.ca AttachmentWincc Flexible 2008 Runtime-connection.pdf (500 Downloads) |
2/16/2011 5:51 PM | |
Joined: 7/28/2010 Last visit: 8/31/2024 Posts: 184 Rating:
|
Hi Ali, Your inhouse system should support a protocol that wincc Flex Runtime can understand, otherwise you won't be able to do it directly. As you can see in the previous document, Flex can talk on DH+, DH485, Modicon Modbus RTU. These are the protocols that run on RS485. If your inhouse system can support any one these then you can make it happen. Unfortunately I don't know of any case that Flex has been talking directly to a third party system. Regards, Behnam www.sigmaprocess.ca |
Follow us on