5/16/2011 6:35 PM | |
Posts: 23 Rating:
|
Hi, I have a problem whereby I can see the colours for Warning and Error in the alarm window but the first colour that appears is the background colour which is defined in Properties/Selection Background Colour. If you click in the window the correct colour appears but for some reason the intial colour is as above and any time you click the alarms window the background colour is active rather than the alarm colour. This is for a TP177B 6 inch colour. Is there another check box somewhere to check Splitted from Different colours on texts in Alarm View . |
Last edited by: O_Moderator at: 5/17/2011 11:36 AMnew subject after splitting |
|
5/17/2011 5:13 PM | |
Joined: 4/29/2010 Last visit: 1/20/2025 Posts: 1557 Rating:
|
Hello, have you activate "use alarm class colors" at the alarm settings? best regards |
5/18/2011 9:16 AM | |
Joined: 4/29/2010 Last visit: 1/20/2025 Posts: 1557 Rating:
|
Okay. Can it be that the colour you mean is the colour of the focus from the alarm view (if a line is marked)? |
Follow us on