12/7/2011 8:24 AM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
The idea is like How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI? WinCC Flex RT and MPI/RS232 Adapter Best regards, Hristo Mihalev |
This contribution was helpful to
1 thankful Users |
12/8/2011 12:55 AM | |
Posts: 50 Rating:
|
exactly my idea is to connect that way, since it only has a connector that connector MPI via a converter cable with RS-485 to RS-232, then exit the converidor I connect with a cable RS232 to USB the question I have is how to parameterize the WinCC flexible RT hardware to link the PC to the MPI, here I put an example, thank you very much for your help
AttachmentDocumento1.pdf (204 Downloads) |
12/8/2011 8:03 AM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
What does the PC recognize in connected USB convertor? Best regards, Hristo Mihalev |
12/12/2011 2:18 PM | |
Posts: 3037 Rating:
|
Hello, you can see in the following FAQ which possiblities of transfer do you have. What transfer options are available in the various operator panels? Tweety |
Follow us on