6/1/2018 3:16 PM | |
Posts: 6 Rating:
|
Hello everyone, I'm writing in this thread because I'm getting the same error message, though unfortunately the cause seems to be different. I'm trying to establish a connection between a PC (Windows 10) running WinCC Flexible 2008 SP5 RT and a CPU 314 via ethernet. When I launch the runtime project, I get the message "connection disconnected: connection_1 <PLC IP address> <rack><connector place>" I've checked the settings both in the Hardware Configuration of Simatic Manager and in WinCC Flexible Advanced (please see attached image). I've also checked the hardware connection between PC and PLC (direct connection with a cable between PC and PLC or using an ethernet switch), disabled the PC Windows Firewall, and verified the setting of PG/PC interface in Windows control panel. This WinCC project worked fine on a previous PC with Windows 7 as OS. Can you please give me any suggestion? Thank you very much! :) ------------------------------------------------------------------------------------------ |
Last edited by: Esk_V at: 6/1/2018 3:28:15 PMLast edited by: Jen_Moderator at: 6/4/2018 7:20:17 AMNew subject after splitting Last edited by: Esk_V at: 6/4/2018 10:52:03 AM |
|
6/4/2018 5:56 PM | |
Joined: 11/5/2012 Last visit: 8/14/2025 Posts: 490 Rating:
|
Hello Esk_V, can you ping your PLC from the computer? Regards. |
6/4/2018 7:28 PM | |
Posts: 6 Rating:
|
Hello Rescobedo, yes, I can ping it. |
6/5/2018 11:42 AM | |
Posts: 6 Rating:
|
Hello Prof. Frink, there's also a "general connection error 0x320" message i didn't notice. Here attached you can find the PG/PC settings screenshot. Thank you! |
6/6/2018 8:36 AM | |
Joined: 7/5/2013 Last visit: 9/12/2025 Posts: 3241 Rating:
|
Hello Esk_V, do you have an onboard-ethernet, too? Are you logged in as Administrator (see https://support.industry.siemens.com/tf/ww/en/posts/wincc-flexible-connection-error/44772)? Regards, Frink |
Pi is exactly three! |
|
6/6/2018 10:01 AM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello, Have you seen this thread: Perhaps a repair of Step 7 or WinCC flexible will do the trick. Best regards, Wizard |
Follow us on