5/15/2018 12:02 PM | |
Joined: 3/31/2018 Last visit: 3/15/2024 Posts: 8 Rating:
|
Hello, Here with HARESH. facing a similar problem in 410 smart controller series, the DI is forced from field and the DI card reads the DI( LED blinks on the card) but I cannot able to see it in Logics/software. The same way just I'm forcing the DO from the program, the bit sets in program and hardware configuration (specific card with monitor&modify option) the bit sets here also. But the command is not coming in DO card( the LED does'nt blinks). what shall i do to sort out this problem.??
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 5/15/2018 1:41:01 PMNew subject after splitting Regards - Haresh KM |
|
Follow us on