9/14/2012 12:55 PM | |
Posts: 93 Rating:
|
Dear Experts, I have 4 HMI runtimes in 4 PCs. Each of the system has a S7300 CPU, I.O modules & Slaves. All these 4 nos of S7 300 CPUs are interlinked (Not in a single network) via PN-PN coupler. So all the CPUs are configured with same I.P address ( SInce the CPUs are not in a network there won't be any I.P conflict), all the Cp343 modules are configured with the same I.P address and PCs with HMI runtime are also configured same I.P address. Even 1st CPU's slaves's I.P addresses are used in 2nd CPU's slaves. Pls refer attached Config-1.pdf Our Customer wanted monitor all the 4 systems in a single system. So we proposed a configuration as i Config-2.pdf. Our plan was to bring all the 4 systems into a single network and monitor via sm@rtaccess.To bring all the systems into a single network, we need to give individual I.P addresses for all the systems. But our customer isn't ready to change the I.P addresses now. Our customer is asking for solution without changing the I.P addresses. So pls suggest me a solution. AttachmentConfigs.zip (174 Downloads) |
Follow us on