10/20/2010 4:35 PM | |
Joined: 9/27/2006 Last visit: 9/4/2025 Posts: 12397 Rating:
|
Hello jmasino; Are you asking whether (and how) it is possible to pass through an HMIand different networks to connect a PC to a PLC? In that case yes, this is possible. In Siemens' world, this is called "routing". The following FAQ will give you details on the configurations required: How do you use WinCC flexible to configure communication between an operator panel and an S7 station via S7 routing? |
10/21/2010 10:52 AM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Dear jmasino, As an addition to DChartier's answer. Perhaps this link might help: Which PROFINET services are supported by SIMATIC panels. If you want to program a CPU through the Simatic Panel, I think it is not possible. Best regards, Wizard |
Follow us on