3/31/2019 11:07 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello, Sinamics DCM 80 is fully digital drive system & has in built checking/testing/diagnosis features. In your case you can set P50380 parameter value as per your requirement which will conduct thyristor check tests as per set parameter value. Apart from this, during running, the in built logic measures various parameters, conducts tests. The measured vaules are readble & user can built up logic to read/display those values. Also drive pops us fault message with fault values (r0949) when the set parameter limits are trigered with its probable causes which guides user to check the causes of fault. Please refer SINAMICS DCM, List Manual, Firmware version 1.3 (based on 4.4) which will help you to understand the working & diagnosis tools available with DCM 80. HTH. |
Last edited by: Jen_Moderator at: 4/1/2019 9:48:03 AMOptimized link. |
|
Follow us on