3/15/2007 7:01 PM | |
Posts: 39 Rating:
|
Hi, You mean to set parameters as following: Tab: Receiving data: Prevent overwriting - DISABLE Delete CP Receive Buffer on Startup - DISABLE ??? Regards Lukasz |
3/18/2007 12:50 PM | |
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
Dear Lukasz, Do you are using the newest P_SEND/P_RECV ? You may find the newest blocks with the software: Download CD "CP340, CP341, CP440, CP441", version: V5.1+SP7 Have you also programmed something to get the STATUS of the SEND and the RECEIVE in a variabele, normally this will be set if there is a ERROR, this bit will however come only one cycle and you have to save the STATUS to see if something is coming into that when you did a call of the block. Normally this error-messages will guide you to a solution. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on