2/15/2024 4:05 PM | |
Joined: 2/7/2024 Last visit: 6/23/2025 Posts: 3 Rating:
|
Hello every one. i have 1. CU250S-2 PN VER. 04-V4.60 2. CU240E- 2PN VER. B01-4.70 3. CU240E-2 PN FW 4.7 SP13 HF4 (purchased just new one) 2 is communicating with laptop via Sinamic starter v 5.5 hf1 with the help of ethernet port and usb cable both (it is for reference to confirm ports and cable) but no. 1 and no.3 are not connecting with ethernet port. but both are working only via USB cable for up loading and downloading program. both LED's are glowing in the start of drive but after a few seconds both are not indicating the connection of cable. anyone can guid me what can it cause. and what is its remedy. Muhammad Danish ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 02/16/2024 09:58:54New subject after splitting |
|
Follow us on