3/28/2019 2:22 PM | |
Joined: 10/11/2006 Last visit: 8/29/2025 Posts: 6037 Rating:
|
Hello, |
With best regards, |
|
This contribution was helpful to
2 thankful Users |
3/28/2019 2:41 PM | |
Joined: 4/2/2016 Last visit: 7/13/2022 Posts: 413 Rating:
|
thanks, I only understood one thing BA - Basic ST - Standard only this but nothing concrete, even concepts Basic and Standard sounds the same... and it only confuses consumers for example why DI 16 x 24 V DC ST (6ES7131-6BH01-0BA0) only available ST (no BA), BUT DQ 16 x 24 V DC/0.5 available ST and BA.... I think it's better to take DQ 16 x 24 V DC/0.5 A ST |
This contribution was helpful to
1 thankful Users |
3/29/2019 10:48 AM | |
Joined: 4/28/2015 Last visit: 8/7/2025 Posts: 399 Rating:
|
Hello, the module ET 200SP, DQ 16x 24V DC/0,5A ST contains more functionality (Diagostics, ...) than the module ET 200SP, DQ 16X24VDC/0,5A BA, like you could see at the technical data of the modules in Siemens Industry Online Support:
Maybe you could also use the TIA Selection Tool to find out the right module for your application:
|
Follow us on