2/25/2025 5:53 PM | |
Joined: 5/24/2016 Last visit: 9/7/2025 Posts: 409 Rating:
|
Hello. Siemens has all of the variables in the SINUMERIK 840D sl NC variables list manual, now be aware this is for the Operate 4.95 system, if you have and older controller some variables might not be available or different. 840Dsl NC Variables List manual You might also be interested in this manual, here on section 4.1 4.1 Flexible NC programming there are several examples in the use of said variables and available commands. SINUMERIK 840D sl NC programming Best Regards |
2/25/2025 6:21 PM | |
Joined: 1/16/2025 Last visit: 3/6/2025 Posts: 7 Rating:
|
Thank you, but going through both of those very carefully I didnt find anything to help with my question/situation above.
|
2/26/2025 12:52 PM | |
Joined: 10/17/2007 Last visit: 9/6/2025 Posts: 4437 Rating:
|
I posted all Siemens documentation link see top 3 tips--picture attached But I have on hand of 840D List for machine builder user. see attachment may meet your needing don't forget the rating if it dose
AttachmentLIS2_0705_en.pdf (161 Downloads) |
Last edited by: nulizhang at: 02/26/2025 19:37:52If you like my comments please |
|
2/27/2025 6:46 AM | |
Joined: 5/24/2016 Last visit: 9/7/2025 Posts: 409 Rating:
|
Hello. You can do either of the ways you described. To have most control I believe you're 1.B solution would be easiet to implement, in this case you can use R variables to use as the input data. Please see section 4.2.3.17 RP: Arithmetic parameter For work offset you have to look at section 4.2.3.12 FU: Settable Work Offset in the NC Var list manual. $P_UIFR is the Translation of a settable work offset. In regards to the setting data from the Jaw section I could not find any information about this in the NCvar manual my self. but I found this reference in some of my other documentation (please see attachment) It says $MAS_SPINDLE_PARAMETER[] and $MAS_SPINDLE_CHUCK_TYPE should be the reference, but I can't test it since I do not have and active setup with as a lathe at this time. Best Regards Riddersholm AttachmentMAS_SPINDLE.zip (134 Downloads) |
Follow us on