7/12/2013 7:29 AM | |
Posts: 261 Rating:
|
Dear all, As per Siemens technical sheet (As link mentioned below) the IM can handle 244 byte of Input Data. http://support.automation.siemens.com/WW/view/en/20132586/td But unfortunately we are unable to insert more than 68 byte. The message coming "The maximum length of the configuration data for a slave with the PROFIBUS address 4 has been exceeded." Can any one guide. Regards, ddg |
7/12/2013 7:32 AM | |
Posts: 1064 Rating:
|
can you post a screen shot node 4 configuration ? |
7/12/2013 7:33 AM | |
Joined: 2/6/2009 Last visit: 9/1/2025 Posts: 940 Rating:
|
[quote user="ddg"]Dear all, As per Siemens technical sheet (As link mentioned below) the IM can handle 244 byte of Input Data. http://support.automation.siemens.com/WW/view/en/20132586/td But unfortunately we are unable to insert more than 68 byte. The message coming "The maximum length of the configuration data for a slave with the PROFIBUS address 4 has been exceeded." Can any one guide. Regards, ddg can you pleas upload your hardware configuration? |
_______________________________________________________________ |
|
7/12/2013 8:02 AM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating:
|
Hello, Please have a look at following FAQ it migh help you. What conditions do you have to comply with when configuring ET 200S modules? |
VANDE MATARAM..... |
|
7/12/2013 8:59 AM | |
Joined: 11/18/2010 Last visit: 8/5/2022 Posts: 523 Rating:
|
Which Module you have inserted On DP slave which casue this problem? VP |
7/12/2013 10:47 AM | |
Posts: 261 Rating:
|
Dear All, Please find the attached file. The IM specification have been attached in previous post of mine. Regards, ddg |
7/12/2013 11:34 AM | |
Posts: 1064 Rating:
|
the configuration data is to large you are going to have to split the node up to get your configuration telegram down in size |
Follow us on