8/16/2011 3:56 PM | |
Joined: 6/24/2008 Last visit: 8/11/2022 Posts: 13 Rating:
|
ThanksSandman, |
8/17/2011 10:07 AM | |
Joined: 5/28/2008 Last visit: 8/31/2025 Posts: 4522 Rating:
|
Hello, If the site engineer doesn't have a WinCC flex. on his PC/PG, then he should use Prosave software. It's free. But with Prosave he will be able to backup, restore or update OS of the panel. He will not be able to modify any thing on the wincc flexible project. So, he should have the image file that he want to download on the Panel. We get this image file when we download a project on the panel and make a backup from this panel using prosave. Thus because, when you use WinCC flexible to download a project, the system compile your project and transfer a compiled file (which we call an image) on the Panel. We can not create this image from WinCC flexible without the existance of the panel. So, please tell us, do you have really an image file to send to the site engineer? And I want to tell that the latest online available version of Prosave isService Tool ProSave V7.4.4 And please note that if you installed WinCC flexible 2008 SP2 + Update 13, you will found that the installed Prosave version is V 7.4.6.0 Hope this helps. |
Ayman Elotaify |
|
8/17/2011 10:13 AM | |
Joined: 4/29/2010 Last visit: 1/20/2025 Posts: 1557 Rating:
|
You can also take a look at this FAQ about Pack&Go. How can you make an indirect transfer with Pack & Go in WinCC flexible? best regards |
Follow us on