8/20/2016 1:27 AM | |
Posts: 21 Rating:
|
Hi Prof. Frink, thanks for answer, I attached the screens the one backup of the program WinCC ASIA, the program its running right now, and i try to take the tags for guide me and i send to you, for you help me. if it does not. tell me for send to you the DB of the PLC. I try to take the tag and convert the hexadeximal value to intiger.
Best Regards Pedro R AttachmentI-O Filed.ppt (288 Downloads) |
8/22/2016 1:19 AM | |
Posts: 21 Rating:
|
Hi Prof. Frink I creted three gauges and three I/O Fields taken the tags fo the WinCC ASIA, I take the DB's, and i linked to every gauge and I/O Field. But the value show in every gauge and I/O Field is too high, in the gaugesthe limit is the 0 to 50 and the 0 to 220 RPM, but in the PLC in the DB 5 DBW 108, DB 5 DBw 60 and MW202, the values are too hig, i need convert that values for the range of my gauges and I/O Fields.
Best Regards. AttachmentGAUGE AND I-O FIELDS.ppt (300 Downloads) |
8/22/2016 7:59 PM | |
Posts: 21 Rating:
|
Hi Prof. Frink, thank for answer. I send to you images from WinCC Flexible and WinCC ASIA. But the last images are the my project in WinCC Flexible, I send to you the images from WinCC ASIA because i have a PC Siemens 627 with the software WinCC ASIA, installed and working with the PLC. and i take the tags from that software, I'm tryingto make a screen in WinCC Flexible very similar. and i taken the tags for my screen but i can not do that gauges work fine. how i do for to make the gauge work's with the DB5.DBW 108 or take or created and modifiy another tag. Best Regards Pedro R. AttachmentGAUGE AND I-O FIELDS 2.ppt (299 Downloads) |
8/24/2016 1:18 AM | |
Posts: 21 Rating:
|
Hi Prof. Frink, thanks for answer. The WinCC ASIA (PC SIEMENS-627) show the values correctly the torque gauge in WinCC ASIA take the tag DB5.DBW 108, and the potentiometer is set to 10 in the control panel, but in my project in WinnCC Flexible my I/O Field shows the value 3109, in my gauge i set the max. value to 50, i think the value show is top to 50 because the value in the tag DB5.DBW 108 is 3109. I wonder if i'm making right the config the gauge and the I/O Field. The connection between PLC and WinCC Flexible Runtime (my project) It is working well.
I wonder if i'm making right the config of my gauge and I/O Field?. I attached the image of my project with the value of the DB5.DBW 108 and 140, and the properties + Scale of my gauge. waiting for your help. Best Regards. AttachmentGAUGE AND I-O FIELDS 3.ppt (264 Downloads) |
Follow us on