3/6/2018 5:39 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Please read 6ra80 what are the required parameters to be enterednin drive to run the motor for testing purpose? to set motor & optimisation parameters. Since your set point is AI 4-20 mA, set p50710(0) = 2, connect set point/reference input to X177:27 & 28. To reverse motor direction you may either reverse the field current/voltage or reverse the polarity of setpoint input. HTH.
|
This contribution was helpful to
1 thankful Users |
Follow us on