9/3/2011 9:56 AM | |
Posts: 327 Rating:
|
Greetings You have to use Set PG/PC. There you can create a new access point, one for Ethernet and one for MPI. Check this thread:/tf/WW/en/Posts/51641#top Best regards
|
Last edited by: fbelic at: 9/3/2011 9:56 AM |
|
9/4/2011 7:03 PM | |
Posts: 327 Rating:
|
Greetings In you project you should have a network configuration something like on picture 1 (two CPUs, two networks, two communication cards in HMI). Then start the Setting PG/PC application and create two new access points, line in picture 2 (e.g. HMI_MPI and HMI_IE). Last, in HMI activate both connections and set access points accordingly. Best regards
Attachmentimages.zip (109 Downloads) |
9/6/2011 1:39 PM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Dear aguere, In addition to the answers of fbelic, Please have a look at this link: Why is the communication driver marked "orange" in WinCC flexible when another Ethernet communication is added to an existing MPI/DP? Best regards, Wizard |
Follow us on