10/22/2012 11:16 AM | |
Joined: 9/2/2012 Last visit: 7/10/2025 Posts: 712 Rating:
|
Dear experts, am facing some problem in alarm configuration. My hardware is TP170b, software is wincc flex 2008 sp2. In HMI alarm view, the date and time showing is wrong( i tried to adjust in panel control panel- but after power restarts again its going to old value- it is 4/8/2010) 1. so I used SFC1, accessed the time from plc succesfully.(plc- 313c 2dp) 2. assigned that same address in area pointer of hmi( see attachment). 3. but after this, am getting alarm event in hmi that " area pointer type: date time plc address error-- error code is 70017." with wrong date and time. 4. but with the same tag, I have configured date and time display field, working well 5. acquisition is configured for 10sec/tried 1min also.But no use.. So please guide me how to overcome this problem Attachmentattachments.zip (199 Downloads) |
|
|
10/22/2012 2:46 PM | |
Posts: 3037 Rating:
|
Hello vipz, You can find a description how you can do a synchronisation with panel an S7 300 in this link. It is attached an example on the end of this link. How do you synchronize the date and time between an operator panel and an S7-300/S7-400 controller with WinCC flexible? Tweety |
This contribution was helpful to
1 thankful Users |
Follow us on