1/13/2019 8:41 AM | |
Posts: 1 Rating:
|
DP/DP Coupler description was useful to show the structure or data needed to exchange under Profibus format but I am seeking for a Siemens file that shows different function that want to send and receive data e.g between S7-1500 and S7-400 programmed with PCS7 or S7. Do you have any sources or you can explain? Specially in PCS7. Thanks We are checking a new Wifi modem which have been embedded in Profibus. Consider that you have a DP/DP Coupler that their interface media are Wifi! Yhey have specific GSD files, and just needed to adjust in program for sending and receiving. between a mobile machine with S7-1500 (TIA V14) and and a fixed main controller S7-400 with PCS7. ------------------------------------------------------------------------------------------ |
Last edited by: abdi517 at: 1/13/2019 8:46:24 AMLast edited by: Jen_Moderator at: 1/14/2019 11:56:06 AMNew subject after splitting |
|
Follow us on