1/20/2012 3:59 PM | |
Posts: 3037 Rating:
|
Hello What do you do with the project? Can you described this? Here is the new Service Pack for WinCC flexible. Service Pack 2 for WinCC flexible 2008 Tweety |
This contribution was helpful to
1 thankful Users |
1/23/2012 7:51 AM | |
Posts: 95 Rating:
|
Hi Tweety, I have attached the PDF file describing the steps which I followed to make a new project in WinCC. I wanted to add SIMATIC MP 377 12" TOUCH in the project but could not.
Hi Hristo, Yup, same problem occurs when I add any HMI. Best Regards, JD Thanks for reply AttachmentWinCCFlex Error filet.pdf (224 Downloads) |
1/23/2012 8:34 AM | |
Joined: 10/7/2005 Last visit: 9/4/2025 Posts: 3049 Rating:
|
Hello JD_techflirt blame Siemens for giving the important WinCC flex templates the rather unfortunate ".TMP" file ending. I had the same happening after doing some automated Laptop "housekeeping" which cleaned up files with ending like these. Anyway, should this be the problem and you have indeeddonethe same "drive clean up", you can fix itby simply copying the '"Template_en.TMP" back over to your PC from another install on a different PC (e.g. from a colleague's PC). If you don't have that,you may find the file on the WinCC flex install CD (not too sure if it exists on in its raw form or if it is embeededin the install package though). I hope this helps P.S: Make sure to exclude the directory that contains this "Template_en.TMP" file from any future drive clean ups (or make a backup copy of it with a different file ending). |
Cheers |
|
This contribution was helpful to
1 thankful Users |
1/23/2012 3:06 PM | |
Posts: 95 Rating:
|
I have a query Regards, JD |
Follow us on