6/26/2013 9:48 PM | |
Posts: 5 Rating:
|
Panels are OP77B and OP177B I don't have panel. I made only runtime. I will try with modification these project, but actualy is dificullt. Resolutions are diffrent on laptop, but this is normal situation, diffrent displays, but resolutions these panels is the same. Look to me file. I made new two example projects, first on dell with flexible sp2 and second flexible sp3 on PG M4, look to text (Tahoma 8), quantity is diffrent on OP77B. I don't know where is problem.Maby somobedy help me. ***************************************** Problem was solved Control panel>All Control Panel Items>Display Smaller 100% AttachmentFile.zip (174 Downloads) |
Last edited by: cameleon79 at: 6/26/2013 10:50 PM |
|
This contribution was helpful to
1 thankful Users |
6/27/2013 11:08 AM | |
Posts: 3037 Rating:
|
Hello, You check this link. http://support.automation.siemens.com/WW/view/en/13899072 You must use small fonts in the setting of your graphic card. Tweety |
This contribution was helpful to
1 thankful Users |
Follow us on