6/13/2011 2:52 PM | |
Posts: 29 Rating:
|
I'm using win cc flexible with v5.3 step 7. Thanks for the reply. Moderator - It is winn cc flexible. |
6/13/2011 6:03 PM | |
Posts: 29 Rating:
|
Made a mistake with error message, wrong problem. Attached screen shot of error. I'm using wincc flexible 2008 which is what the machine builder used. Problem I think is in the version of step 7 which, I'm sure, the machine bulider was using v5.4. We have v5.3. Have tried to get the original project from m/c builder but this would not be of much use if the step 7 versions are different as explained below.(This is info I have been told) When the project was created a log.idf file is created (which I can not find) to match the hmi. file. As the m/c builder is using v5.4 the log.idf will not open with v5.3 , that's how I understand it.....I think. I posted this same fault some months ago but did not get anywhere with it. I was told to delete the log.idf file and when the flex project is opened a new log file would be created. I could not find the log.idf file ? If someone could point me in the right direction of this file I would be greatful. Attachmentsqlserver.zip (147 Downloads) |
6/14/2011 9:39 AM | |
Posts: 29 Rating:
|
Have managed to open the project. Archived the project, retrieved and now opens ok ? |
Follow us on