10/9/2017 3:37 PM | |
Posts: 2 Rating:
|
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/10/2017 7:24:33 AMNew subject after splitting |
|
10/9/2017 6:25 PM | |
Joined: 11/29/2011 Last visit: 2/4/2025 Posts: 1362 Rating:
|
Hi, You seem to have a hardware interrupt enabled in your HW config, but your code do not have the associated HW interrupt OB. Further info about HW interrupt in What is a hardware interrupt and how do they work in the S7-400 system? You could consider two options: implementing code into OB40, or disable the hardware interrupt on the card. See the highlighted text below. Event 1 of 120: Event ID 16# 35A1 |
- What you read here, please check with manuals and your requirements. |
|
10/9/2017 8:29 PM | |
Posts: 2 Rating:
|
Thank you. now the machine is working, but the EXTF light is on in CPU. I can not define the issue.before I download the OB40, the EXTF is still on. No relevance for user (Z1): 0016 DO YOU KONW WHAT IS MEANING OF 0016? AttachmentDiagnose.txt (405 Downloads) |
10/9/2017 11:24 PM | |
Joined: 11/29/2011 Last visit: 2/4/2025 Posts: 1362 Rating:
|
Hi, I did not get the chance to look at buffer anyways... EXTF means that An external error was detected, that is, the cause of error is not on the About OBs.. Have a look at the Which organization blocks do you need for error handling in STEP 7 V5.5? FAQ for overview. Make sure the fault OBs are downloaded to prevent further Stop events. I hope I could help! |
- What you read here, please check with manuals and your requirements. |
|
Follow us on