1/21/2018 9:42 PM | |
Joined: 9/27/2006 Last visit: 9/9/2025 Posts: 12401 Rating:
|
Hello walid; Look at the attachment below: the S5 adapter is part of the S5 module you want to install in the S7 rack. To find the information you need, you must know the type of S5 module you want to install, the look for the manual for that module; information on the installation in a S7 rack should be in the appendices. S5 modules that can be implemented in the S7-400 system using the adapter Manual for the IP 240, with appendices on the S7 adapter case (Manual for IP 240 counting/positionning module, English, MLFB 6ES6998-0TB22 (search for this part number on the web)). The screenshot below shows the start of the Appendix 2 of the manual for IP 240, installation and configuration of the IP 240 in a S7-400. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 1/21/2018 9:43:15 PMLast edited by: Jen_Moderator at: 1/22/2018 8:14:44 AMInserted right links. |
|
Follow us on