1/13/2009 7:44 AM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello mandy, To have access to change parameters you must first change P060=7. After P462 and P464 is for acceleraion/deacceleration time which time is important in Start and Stop command. The acceleration time relates to an acceleration of 0 to 100 %. The deceleration time relates to a deceleration from 100 % to 0. You want to change he speed. For this is necessary to say how you will control this drive. You have Profibus connection (sepoint for speed is receive from Profibus Master) or control via analog potenciometer conneced to the terminals of the drive, or with fixed sepoint (P0401). For more details I suggest you to read SIMOVERT MASTERDRIVES Motion Control Compendium (MC 2.4) Search there "setpoint" and you will see how can be connected this value with start and stop command. Of course there has explanation for making 2,3... setpoints that can be switch on. I hope help you. regards |
1/15/2009 2:00 PM | |
Posts: 1 Rating:
|
hi mandy82_india |
Follow us on