2/26/2011 8:56 AM | |
Posts: 153 Rating:
|
Nuremberg, Germany, 2011-Feb-23 A new range of Logo! logic modules has been equipped by the Siemens Industry Automation Division with an integral Ethernet interface. The two new basic devices Logo!12/24 RCE and Logo!230 RCE with communication and network capabilities enhance the Siemens portfolio with logic modules geared to meeting demanding applications. The performance of the new basic devices has also been significantly improved, for example the program capacity has been doubled to 400 function blocks, and a wide range of new practice-oriented functions has been introduced. These include macro functions for recurring program sequences, and data logging functions for documentation and evaluation purposes. Up to eight of the new logic modules can be networked using standard Ethernet switches. Together with the Ethernet interface and the new SD card reader, the new modules have a width of six MW (modular width) and thus 108 millimeters. The standard devices with a width of four MW are still used for simple applications. 1)http://www.siemens.com/press/en/presspicture/2011/industry_automation/IIA2011022520-01.htm 2)http://www.siemens.com/press/en/pressrelease/index.php?content=automation AttachmentIIA2011022520e.pdf (1270 Downloads) |
Last edited by: Andres [Str] at: 2/27/2011 1:25 PMLinks from pdf-file are added Last edited by: Andres [Str] at: 2/27/2011 1:17 PM |
|
This contribution was helpful to
6 thankful Users |
4/7/2011 11:38 AM | |
Posts: 24 Rating:
|
The new one seems relay nice !! Someone knows when it will be available?? |
4/7/2011 5:35 PM | |
Posts: 3 Rating:
|
i heard rumors that it would be released this summer... the sooner the better, my fingers are itching for it! |
4/7/2011 9:44 PM | |
Posts: 153 Rating:
|
Hi all. The information about modules has appeared on a site LOGO! Logic Module |
Last edited by: Andres [Str] at: 4/20/2011 4:59 PM |
|
4/28/2011 11:58 AM | |
Posts: 204 Rating:
|
Thanks for this information we need more and more................. |
4/28/2011 4:42 PM | |
Posts: 12 Rating:
|
Hi guys!....interesting... when will these be availabe in asia? particularly in the philippines? |
4/28/2011 4:52 PM | |
Posts: 2930 Rating:
|
Hi all, at Hanover fair Siemens told me beginning of July is delivery release planed. hope this helps |
Follow us on