7/7/2013 3:47 PM | |
Posts: 8946 Rating:
|
I = P / U P = U * I R = U / I |
7/7/2013 5:01 PM | |
Joined: 5/28/2008 Last visit: 9/3/2025 Posts: 4522 Rating:
|
Dear all, From the given data, all the above solution may be correct. Coz every body including myself put his assumption. kinjalpatel1899did not told us if it is 3 phase circuit or not. SoVithani'sAnswer is correct if it is 3 phase circut and ifkinjalpatel1899have some other loads connected with the capacitor bank. I mean if it is not a pure capacitor bank load. And in this case you need to know power factor. Navnaganswer is also correct if it is a pure capacitor bank. In this case Sin Phi = 1. |
Ayman Elotaify |
|
This contribution was helpful to
1 thankful Users |
Follow us on