5/23/2023 11:50 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
how is this related to SIMOTION? |
5/23/2023 12:27 PM | |
Joined: 5/23/2023 Last visit: 7/22/2025 Posts: 3 Rating:
|
You are right,is not related... in which section would it be more appropriate? |
5/24/2023 5:03 AM | |
Joined: 3/11/2019 Last visit: 9/1/2025 Posts: 1653 Rating:
|
Hi, it also depends on which f-modules you are using and how they are configured. S7-FCT e.g. will only work if the modules like ET200SP were configured via GSDML file. If they were configured via integrated hw-catalog, S7-FCT won't work. Maybe this can help: How do you assign the associated PROFIsafe addresses to the F modules of the ET 200SP without additional Engineering?regards sancruz |
Last edited by: sancruz at: 05/24/2023 05:04:23Feedback appreciated, please rate |
|
Follow us on