10/2/2011 10:00 AM | |
Posts: 148 Rating:
|
I need to build a new hardware interface in siemens rack (VHDL at FPGA board) I need amanual discribe the backplane communication |
10/5/2011 9:31 AM | |
Posts: 148 Rating:
|
up |
10/5/2011 4:21 PM | |
Posts: 148 Rating:
|
I think I need the P-BUS information to control the I/O card ?
and also Backplane bus in S7-300 and S7-400 |
10/6/2011 2:21 AM | |
Joined: 10/7/2005 Last visit: 9/14/2025 Posts: 3049 Rating:
|
Hello AmirAlwaled I'd say you can rest assured that the backplane P-bus (I/O bus) protocol is Siemens propietary and also that there are differences between the S7-300 and 400 at least as far a thebackplane K-bus (communication bus) is concerned (none of which will make your task any easier I'm afraid). One additonal pointer I can give you though is to read Decinteresting research into this subject in the thread informations about backplane (S7 300 related). While this, together with the other info you found, may give you enough starting points to do the reverse engineering of the backplane protocol, you will still have your work cut out for yourself. Saying that, "value added third party" modules from other companies do exist (e.g. Helmholz offers CAN bus modules for the S7-300 which don't exist inthe Siemens portfolio) and these companieswould have the knowledge of the backplane protocol and may (but possiblymay not) be willing to share it. My question to you is though: Is it a must have that you hook your product/module onto the S7 backplane? It may not only be easier, but would possibly also open you development to a wider market, if you instead develop it as a standalone module withlet's say Profibus or Profinet interface (which are open andwell documented interfaces). Food for thought anyhow and I hopeit helps. |
Cheers |
|
This contribution was helpful to
3 thankful Users |
10/16/2011 11:14 AM | |
Posts: 148 Rating:
|
That is right
It's a great post from Dec I should PM him
I have already communicated with VIPA but "Frau Kuefner" transferred me twice to egyption sales partner I will tray to counicte with ILStechnology that devolop " Siemens CP 343-1 ERPC " . and you have add Helmholz to my list thank you again
Yes you are completely right. but I am developing it first " for fun For example there is aggregate Servers from HP called " HP Blade ". We have four of them each are 2 Xeon processors 2.4 GHz 8 cores each, 24 G ram,10 G NIC , with great redundant ,HP 4400 Enterprise Virtual Array,HP SAN Switch, Cisco Core switches , Symantec Backup Exec System Recovery , But we can't use it with WinAC because there is no CP1616 for Mezzanine interface |
This contribution was helpful to
1 thankful Users |
10/16/2011 8:29 PM | |
Posts: 148 Rating:
|
cancel the project I am waiting 17 october to begin again with "Willi Heintz" VIPA Vice President.and I will try with ILStechnology , and Helmholz also. I am waiting Dec response also. I wasting my time in usual working and preparing to lead two another teams in " INDAC Egypt 2012 "one of them will be a WinAC project and I think it will be this example : Linking Windows Applications to WinAC RTX with WinAC ODK Using the Example of SIMATIC Vision Sensors. but I have to change SIMATIC Vision Sensor "VS 723" with cheap camera because of the high cost (about 4000 EUR) |
Last edited by: AmirAlwaled at: 10/16/2011 8:30 PM |
|
10/18/2011 6:43 PM | |
Posts: 148 Rating:
|
I need to develop interface to control the Step7-300 I/O Modules from a PC ( without the PLC CPU Unit)I will use VHDL language on Xilinx Spartan-3 FPGA (I think it will be enough) PC(USB for Ex.) ---> I/O Moudule (Backplane). PC(USB)-->(USB)Xilinx Spartan-3 FPGA(serial)-->(Backplane) Step7-300 I/O module.
I think that I need P-Bus Protocol and how to send the configuration from the PC to I/O modules.Am I right? Now I need to know what you know about that ? Thanks because you give me information about what I have to know if I decide to develop CP Module ,Knowing what you have to know is the first step always. |
Follow us on