4/2/2021 12:33 PM | |
Posts: 8 Rating:
|
Hello, I have IOT2050 Advanced and try to do first setup. I was able to connect with cable to console port,change boot order but can't boot to any system. I tried both example image and IndustrialOS, both USB and MicroSD, two different cards and three different USB sticks. With IOS the reboot comes here:
Same from SD card and USB. With example image it is starting boot, but crash after USB check (even with sdcard boot):
Full logs and env_print are attached. Attachmentenv_print.txt (565 Downloads) |
4/2/2021 12:34 PM | |
Posts: 8 Rating:
|
Log of Example image from SD card
Attachmentexample_boot_sdcard_log.txt (555 Downloads) |
4/2/2021 12:35 PM | |
Posts: 8 Rating:
|
Log of IOS from SD card
Attachmentind_os_boot_sdcard_log.txt (605 Downloads) |
4/2/2021 12:35 PM | |
Posts: 8 Rating:
|
Log of IOS from USB
Attachmentind_os21_boot_usb_log.txt (569 Downloads) |
4/8/2021 1:38 PM | |
Posts: 8 Rating:
|
No. Of course I would test it before if I have any other IOT. |
Follow us on