6/24/2009 11:55 AM | |
Posts: 24 Rating:
|
Dear All, I have a problem about parameters download from my PG to CUVC. I can upload all parameters without any problem from CUVC to my pg.But when I start to download parametersto cuvc some parameters is rejected.You can find parameters in attached file. I have searched this site ,it is mentioned P053 parameter and power defination. I removed all in/output sockets also profibussocket , also I changed p060 parameters,but i can not manage. Could you please send any suggestions ? What shouldI do? Attachmentm2013-01-contact roll.zip (392 Downloads) |
6/24/2009 12:53 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hi, Perhaps this FAQ could be helps Masterdrives DriveMonitor: Interface release for P053, P927 Regards Hristo Mihalev |
6/25/2009 11:15 AM | |
Posts: 160 Rating:
|
You should have a log file that you can save that lists which parameters did not donwload, can you post it here please. |
6/27/2009 8:32 AM | |
Posts: 160 Rating:
|
Hi To connect via Drivemonitor to the CUVC via the PMU please find attached the connection scheme for the cable to use for this purposefrom your PC |
7/20/2009 7:10 PM | |
Posts: 24 Rating:
|
please, copy log file from downloading params to driveand paste it in here. |
Follow us on