8/2/2022 8:41 AM | |
Joined: 7/28/2022 Last visit: 10/13/2022 Posts: 5 Rating:
|
Hello, I am having problems with the iot2050 basic fs02 firmware 1.02.01, when booting with the keyboard and the monitor connected nothing appears and I try to boot from putty through UART and I get information about the device but later from that the red led light jumps and it does not let me execute any command from putty and they are written as scribbles instead of normal letters, and I would like to know if I really have the operating system installed correctly or not, I also tried to perform it by ethernet following the steps but it doesn't detect it. Thanks and regards. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/02/2022 11:41:29New subject after splitting |
|
Follow us on