1/2/2025 10:20 AM | |
Joined: 7/10/2024 Last visit: 8/22/2025 Posts: 180 Rating:
|
Hello! I recommend you try it in simulation, because if it works like this, it is probably due to the difference in operating system between the HMI and the computer you simulate on. The simulation uses some resources of the Windows OS on which it runs, but on the Panel there is Windows CE, which has limited functionality. So this may be a limitation of the HTML Browser object in the Basic Panel, since it is limited for the display of simple HTML pages. Try the following FAQ to verify that the HTML Browser object works in this specific application? - How do you display screens from a USB stick in the HTML Browser Control on a Basic Panel 2nd Generation? - https://support.industry.siemens.com/cs/es/en/view/109482823 |
If you found this post helpul, I'd greatly appreciate your feedback with the rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on