12/21/2022 7:34 AM | |
Joined: 1/21/2013 Last visit: 9/12/2025 Posts: 4108 Rating:
|
Hi Just_Starting, SIMATIC ET 200 is the decentralized I/O system from Siemens. It is supplied optionally with PROFINET or PROFIBUS interface and works together with different PROFINET IO controllers or PROFIBUS masters, also from different manufacturers (except some failsafe components). So you can use it with S7-1200, S7-1500, S7-300 or S7-400. It does not matter wheater you are using a modern PLC or an older one. The main advantage of the new generation is: It's new! Siemens - of course - did some imporvements on the systems. And the new generation will be available also when the old generation is discontinued. Kind regards |
12/21/2022 2:07 PM | |
Joined: 4/28/2015 Last visit: 4/19/2025 Posts: 10876 Rating:
|
Hello, did you look at my recommended TIA selection Tool? Can it help you? Cloud: TIA Selection Tool Cloud cfg |
Last edited by: Duris_I at: 12/21/2022 14:14:34With best regards... |
|
This contribution was helpful to
1 thankful Users |
Follow us on