8/13/2010 12:03 PM | |
Posts: 134 Rating:
|
www.siemens.com/s7modbus Is this the link..you are talking about dear.. |
8/16/2010 9:15 AM | |
Posts: 3093 Rating:
|
yes, this is the link |
8/16/2010 7:49 PM | |
Posts: 3093 Rating:
|
Hello Patel, you can download the wizard here: http://support.automation.siemens.com/WW/view/en/31535566 You can find this link also in the manual of ModbusPN. Regards, Kaulquappe |
This contribution was helpful to
1 thankful Users |
8/18/2010 1:16 PM | |
Posts: 134 Rating:
|
Hi.. Thanks for the reply.. Now i have one problem..according to pdf available on these links,i understands that if i want to hook up IM 151-8 PN/DP with GATEWAY on IE, i need to go for MODBUS TCP... Is there any alternative..? Another problem is i dont have purchased genuine licence for S7 OpenModbus/TCP Software ...currently i have downloaded demo version from site because its urgent. Now, how long can i use this demo software without any problem?What problems i have to face if i continue with this demo. |
8/18/2010 4:42 PM | |
Joined: 9/27/2006 Last visit: 9/8/2025 Posts: 12401 Rating:
|
Hello paytel; I don't have the answers to these questions. User Wustenrauber seems to be the expert on IT4Industry, developpers of the Open Modbus/TCP package. He might be able to help you more, either through this thread or by private message. Hope this helps, Daniel Chartier |
8/18/2010 5:34 PM | |
Joined: 10/3/2008 Last visit: 7/31/2025 Posts: 996 Rating:
|
Hi, I don't know any other possibility to connect the IM151-8 PN/CP to the gateway. The demo version has no time limitation. The "restriction" is a blinking SF/INTF-LED, some entries in the diagnostic buffer of the CPU and a status A090 on the modbus block. The modbus communication is running always. Wüstenräuber |
This contribution was helpful to
2 thankful Users |
Follow us on