3/29/2023 8:04 PM | |
Joined: 6/26/2019 Last visit: 6/24/2025 Posts: 22 Rating:
|
Hello, IOT2050 Advanced FS:02 09.2021. I can´t boot with v1.1.1 image from sd in order to upgrade firmware. It's hangs at serial cable driver (see atached file) [ 3.350174] usb 1-1.4: new full-speed USB device number 3 using xhci-hcd [ 3.455854] usb 1-1.4: New USB device found, idVendor=10c4, idProduct=ea60, b cdDevice= 1.00 [ 3.464202] usb 1-1.4: New USB device strings: Mfr=1, Product=2, SerialNumber =3 [ 3.471505] usb 1-1.4: Product: CP2102N USB to UART Bridge Controller [ 3.477940] usb 1-1.4: Manufacturer: Silicon Labs [ 3.482641] usb 1-1.4: SerialNumber: defb5adad735eb11b841d8d74e5d922d Only boot with old v1.0.2 but it's not posible to update firmware. It's unusual that with de v1.2.2 from sd boot, but don't charge network environment and don't reconoced emmc. I tried with several serial cable and sd cards. It is posible to recover it? NOTE: setenv boot_targets is changed to microSD boot first. Attachment20230329_COM_OUTPUT.txt (610 Downloads) |
Follow us on