12/9/2022 10:50 AM | |
Joined: 8/3/2009 Last visit: 9/5/2025 Posts: 16348 Rating:
|
Hello GTSAGarcia you can use both but without the Option+ you need SMB V1 in Windows System where the share is located. If your IT does not allow these older Security then you have to go with Option+ https://support.industry.siemens.com/cs/ww/en/view/92346478 Bye Murof |
If this Information really helps, you could use the Rate function |
|
12/10/2022 10:32 AM | |
Joined: 6/1/2020 Last visit: 8/21/2024 Posts: 41 Rating:
|
Thanks for the suggestions. Then I will try to ocnfigure HMI Optons+ to copy the CSV files in the server. |
2/14/2024 9:54 AM | |
Joined: 8/3/2009 Last visit: 9/5/2025 Posts: 16348 Rating:
|
Hello JiriSv It would be nice if you give us a few more information (which panel, which versions, which Image version ,which OS where the Share is located) the Option + Manager works without SMBv1 But you cannot have direct access to the path like without the Option+ Manager (this will need SMBv1): https://support.industry.siemens.com/cs/ww/en/view/92346478 Bye Murof |
Last edited by: Murof at: 02/14/2024 09:54:25If this Information really helps, you could use the Rate function |
|
Follow us on