12/13/2023 1:12 PM | |
Joined: 12/18/2014 Last visit: 9/2/2025 Posts: 35914 Rating:
|
Can you please upload your LOGO! program as a ZIP file? |
12/13/2023 4:14 PM | |
Joined: 12/21/2021 Last visit: 4/22/2025 Posts: 6 Rating:
|
Hello Hazard and ixo, I've added the project in a zip file and here is a screenshot: For completion I added the CIM settings. Communication functions for the S7 and the MODBUS RTU. The problem is as followed:
These valeus are used to determine wether a generator should be activated or not. When the power consumption is above 30kW the generator should be started. When the power consumption drops below this value, the generator should be disconnected and turned off. Because the power consumption values might not be updated due to physical damage to the MODBUS communication wires the generator will not turn off when the power consumption drops below 30kW.
I hope this clears something up! Kind regards, Ard AttachmentProject.zip (489 Downloads) |
Follow us on