11/21/2024 9:34 PM | |
Joined: 7/29/2022 Last visit: 8/15/2025 Posts: 6 Rating:
|
Dear All, I have 6 networked LOGO controllers (a combination of V8.3 and 8.4) Controller 3 (v8.4) sends out a signal over the network to Controller 6 (v8.3) to switch an output Q2. The Output Q2 on controller 6 has been switching on and off (once every 3-5mins) even though the input signal from controller 6 is continuiously on. When testing this in 'online mode' (see attached screenshots) you can see the network signal from controller 3 as always red however the input signal to controller 6 switches between red and black. I have completed some IT network tests over a 15min period and this shows zero packet loss Please can anyone tell me why the networked input signal to controller 6 keeps switching on and off whilst the network signal from controller 3 is constantly on? Many thanks in advance. Attachment2024-11-21 Heating Controls.pdf (169 Downloads) |
11/22/2024 3:05 AM | |
Joined: 12/18/2014 Last visit: 9/4/2025 Posts: 35918 Rating:
|
Which firmware has the LOGO! 8.4? The current firmware version is V1.84.03. If your firmware version is not V1.84.03 then update the firmware. The update can you download from here: Firmwareupdate für LOGO! 8.4 Grundgeräte und Service Pack 1 für LOGO! Soft Comfort V8.4 |
11/22/2024 11:50 AM | |
Joined: 12/18/2014 Last visit: 9/4/2025 Posts: 35918 Rating:
|
No idea. Ask Siemens via Support Request. |
11/22/2024 2:05 PM | |
Joined: 12/18/2014 Last visit: 9/4/2025 Posts: 35918 Rating:
|
No. Start a Support Request and ask Siemens directly. |
11/22/2024 2:42 PM | |
Joined: 7/29/2022 Last visit: 8/15/2025 Posts: 6 Rating:
|
Controller 5 now FW 1.84.03 No change with issue Thanks |
Follow us on