1/13/2022 9:07 AM | |
Joined: 8/3/2009 Last visit: 9/3/2025 Posts: 16293 Rating:
|
Hello ntokas I would try to delete the IM folder in the project (first enter the correct computername in the project): https://support.industry.siemens.com/cs/de/en/view/109778709 then download the Project to a different location as before (different folder). Then try to run again. Bye Murof |
If this Information really helps, you could use the Rate function |
|
1/14/2022 11:54 AM | |
Posts: 3 Rating:
|
Dear Murof, Thank your for your suggestion. I tried to do exacly as you said, however the same problem persists. I took some screenshots, as you can see at the .zip file. The names of the pictures describe what is about. It' s about the state of the SQL server before and after deletion of the IM (i installed SQL Server Management Studio for this). Also, it's about the state of the SQL Server Configuration Manager, which has exactly the same state with the one in the working ok pc. Is it a good solution to try and uninstall the SQL Server and reinstall it with the TIA Portal installation ? Also, which version of the SQL Server and related programs should be uninstalled ? Or if there are any other suggestions, they are more than welcome. Thanks again for your time. Attachmentfaulty database pc.zip (336 Downloads) |
Follow us on